Configure Onboard I/O
The procedure to define the local I/Os of the AKD drive In electrical engineering, a drive is an electronic device to provide power to a motor or servo. Control device for regulating the speed, torque and position of a motor. A unit controlling a motor using the current and timing in its coils. is very similar to the one for I/O slices, with these exceptions:
- Channel column also contains in brackets the connector and pin number.
- PLC Programmable Logic Controller - A digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines.
Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events. variable selection applies to digital inputs and analog inputs and outputs.
- See Map I/O from the Project Explorer for more information.